contactusurl/en/marine-and-infrastructure/searchNo ResultsAnimation is not fully supported in Internet Explorer versionsitem founditems founditem founditems foundofSearch & HelpShowingOn this pageYour Browser is outdatedDealerDistributorOfficial DealerPremium PartneraddressaddressesArticlesRegulatory Press Release,Regulatory press releases onlyEG. Food Hoses conformity evolution WebinarSelector Button
Trelleborg helps ship owners and crew alike manage ship performance and efficiency over the entire voyage, right down to the final 200 meters.
Ship Performance Technology
Trelleborg Marine & Infrastructure has been developing marine electronic systems, including Ship Performance Monitoring Systems for over 30 years. These systems can provide operators and owners with huge fuel savings.
On 17 June 2021, the International Maritime Organisation (IMO) adopted amendments to MARPOL Annex VI at MEPC 76, introducing regulations 23 and 25 – The Energy Efficiency Existing Ship Index (EEXI) and Operational Carbon Intensity Indicator (CII), which are the first steps for the shipping industry to move towards its target of zero carbon emissions by 2050, compared with their level in 2008.
Prepare Your Fleet For EEXI Compliance with TSX5 & ECO8 ShaPoLi
To meet the requirements of the MARPOL regulation, Trelleborg teamed up with EDIT Automation, Greece to develop a ShaPoLi system, which is both cost-effective and user-friendly.