High Performance Automotive Coated Fabrics for The Road Ahead
Our constant desire to innovate is what drives us to continuously meet the needs of major automotive manufacturers with our customized polymer-coated material solutions.

Reevecote® by Trelleborg
For the mechanical sealing of fluids and gases to prevent leaks or as a barrier between two objects such as metals and gases/chemicals, use Trelleborg REEVECOTE® .
For more informations, click here or drop us a line at ECF@Trelleborg.com
Coated Fabrics that Help Make Next Generation Electric Cars a Reality

The quest for an electric car that will be adopted in volume has intensified as manufacturers seek to lower CO2 emissions and retain vehicle access in some of the world’s most-populous cities. Engineered Coated Fabrics continuously works to remain at the forefront of innovation.
Do you have an e-mobility project that could benefit from coated fabric technology, such as drive belts, firewall FR protection, thermal barrier for battery compartment, or electrical insulation / protection?