Globe Trotting

After relocating from India to England, Inderjeet Singh has shifted his focus from seals with complex designs to seals made of innovative materials. But he says the principles of product management are the same the world over.
- By Donna Guinivan

IN SHORT
- Inderjeet Singh has relocated from India to the UK
- He discusses the similarities and differences between working in Bengaluru and Tewkesbury
- He is now responsible for promoting Isolast® globally within Trelleborg Sealing Solutions

Isolast® materials are the gold standard among elastomers. Differing from other rubber compounds, they are chemically resistant to virtually all media while demonstrating outstanding performance.
The benefits of perfluoroelastomers (FFKMs) can outweigh their often seemingly higher cost as they can operate at temperatures up to +320 °C / +608 °F for long periods in the harshest of process media. These include the aggressive chemicals employed in the cleaning and sterilization regimes used in food production that can potentially destroy a standard seal in hours.
In many cases, FFKMs are the only option in critical aerospace or oil and gas applications. And with the ability to manufacture and pack in class 100 and class 10000 cleanroom environments, seals can be supplied to meet super-clean requirements, such as for semiconductors, where the slightest contamination can destroy an electronic product.