Minimum Friction Maximum Performance

Date: 06.02.18
For years, professional athletes have been coating their ski and snowboard gear with ultrathin coatings that provide exceptional glide properties. Surface coatings at nano-scale are not only for winter sports anymore. Seal-Glide®, an innovative surface treatment from Trelleborg Sealing Solutions, significantly improves friction and stickslip properties of elastomer seals while having little or no effect on the performance of the compounds the seals are made from.-By Donna Guinivan

IN SHORT
- The Seal-Glide® process allows seals to be coated thinly to just a few hundred nanometers
- Two versions are available; Seal-Glide® Nano for general applications and Seal-Glide® Medical for healthcare applications
- Advantages of the coating includes low friction and enhancing automated processes
“The Seal-Glide® Medical coating is ideal for use in healthcare and medical applications as the new process has a very high level of stability.”
ANDREAS SCHMIEDEL,
Technical Manager for Healthcare and Medical in Europe at Trelleborg Sealing Solutions
Technical Manager for Healthcare and Medical in Europe at Trelleborg Sealing Solutions

THE SEAL-GLIDE® RANGE
Currently there are two coatings in the Seal-Glide® range:
Seal-Glide® Nano for general applications.
Seal-Glide® Medical for healthcare applications.
Further coatings will be added in the future
Seal-Glide® Nano for general applications.
Seal-Glide® Medical for healthcare applications.
Further coatings will be added in the future
“Another advantage of Seal-Glide® is that due to its thinness, the coating has a high level of transparency and does not cover the original color of the elastomer.”
-GORDON MICALLEF, Operations Director at Trelleborg Sealing Solutions in Malta