Technology Applied Damping Material


“We’ve developed a completely new material for inverters because they make a wider range of noise,” says Arvid Norberg, Director of Sales and Marketing for damping solutions at Trelleborg. “By combining a different thickness of metal with different types of polymer thickness you can have a higher level of damping at a wider noise frequency and temperature.”
The exact material composition is secret. Suffice it to say, the polymers are based on nitryl butadiene rubber (NBR), and the adhesive is typically an acrylic, though other materials can also be involved.
But it’s a challenging development process because electrical engines and drives have even tougher cleanliness standards than combustion engines.
“The most critical thing is that there are no loose metallic particles past a certain size, as these can get into the engine or even the electronics and cause a short circuit,” Axelsson says. “We are asked to control the level of particles on the parts we supply.”
Norberg adds, “We’re talking about tenths of millimeters that are often invisible to the naked eye.”

With the growth of e-mobility, Norberg believes ADM has significant market potential. It underlines the decision of Trelleborg Sealing Solutions several years ago to diversify from brakes and solidify its market-leading position in damping solutions. The team working in this area is growing too.
“We are at the forefront of the market, and we see e-Mobility as being very important in the years ahead,” says Norberg.
So how will the technology develop? “We’re using more lightweight materials wherever possible,” says Axelsson. “Our focus is noise and vibration, but we are also looking to see how we can respond to other new requirements that come from our customers.
There are also new workplace directives on noise from the European Union to consider. The health and safety requirements regarding noise and vibration are only getting tougher, but that’s good for us as we’re regarded as the leading developer of brake and damping products.”
With the possibility of this technology being used in other industries, such as consumer electronics, it’s clear that ADM has enormous potential, keeping Trelleborg ahead of the competition.