The e -Team


- A major obstacle to widespread electric vehicle adoption is being unable to achieve the same range as gasoline-powered cars.
- Trelleborg Sealing Solutions assembled an agile rapid-response team of engineers and other experts to address growing customer demand.
- Two new products specialized for e-axle applications have been released – HiSpin® PDR RT and HiSpin® HS40 – the result of the team's work.

THE E-AXLE
Often described as eAWD, the e-axle is an electro-mechanical propulsion system contained in an axle structure housing an electric motor, the power electronics and some form of gearing/differential.
Scan the QR Code to find out more

The advantages of electric vehicles are not just confined to sustainability but health protection too. Though limited international statistics exist, according to the World Health Authority about 40% of the population in EU countries is exposed to road traffic levels exceeding 55 db(A), while 20% is exposed to 65 db(A).
These noise levels are considered detrimental to health. Electric vehicles are one of the solutions that could cut down urban noise. For example, a low-floor, diesel-driven bus starting from a bus stop would emit 72dB of noise, while the equivalent electrically driven vehicle would emit 56dB.

Introduced in the 1940s in response to a shortage of cart horses and a need for increased efficiency, the electric milk float became a welcome and familiar sight in the streets of the U.K.
In August 1967, the U.K. Electric Vehicle Association put out a press release stating that Britain had more batteryelectric vehicles on its roads than the rest of the world put together and almost all of those were milk floats.

RANGE ANXIETY
“Our aim for the new eMobility seals was therefore to increase operating rotational speed to at least 40 meters per second.”

Trelleborg Sealing Solutions has been involved with electric vehicle development since their inception. Working closely with our customers, Trelleborg realized there was a need for specialized sealing solutions that could help increase the distance per charge of an electric vehicle.
The eMobility seal project was convened in November 2017 and a special multi-disciplinary team involving R&D, engineering, product management, manufacturing and sales was put to task to rapidly find a solution that could support the evolving electric vehicle sector. This was ready for launch in July 2018.

MORE INFORMATION
Tech Talk: HiSpin® for e-Axles
Check out the newest addition to our Technical Library: a Tech Talk on High Speed Rotary Seals for Electric Drive Units. Our online Technical Library features a collection of in-depth lectures, webinars and whitepapers on innovations in sealing technology.
Specialized eMobility Sealing Solutions

Trelleborg Sealing Solutions has developed two high performance seals specifically for the e-axle in electric vehicles, a combined electric motor and gearbox that fits within the traditional axle/ differential space. The motor and gearbox are directly coupled but while the gearbox requires efficient lubrication, it is essential that the motor remains dry and so a highly reliable seal is required between these two components.
The two seals have exactly the same functions and the choice between the correct seal to specify is dependent on the operating parameters of the e-axle system.

Key characteristics
- Constructed from two parts: a precision manufactured metal body and a mechanically retained Turcon® sealing element
- Custom-designed Turcon® lip with concentric slit features to improve performance of lip laydown profile on shaft, crimped into a precision machined body
- Combines the advantages of Trelleborg’s proven Turcon® grade PTFE materials and proprietary RT Technology

- Familiar product type to automotive customers
- Unique bi-directional hydrodynamic lip feature with negligible frictional torque at high speeds
- Rubber lip geometry and flexible design for optimum lip contact on the shaft as a result of extensive FEA studies
- Manufactured using proven proprietary XLT Fluoroelastomer (FKM) compounds to meet higher speeds and a wider operating temperature range and increasingly aggressive synthetic Automatic Transmission Fluids (ATF)
- Produced using proven conventional high volume manufacturing processes
- Manufactured using proven proprietary XLT Fluoroelastomer (FKM) compounds to meet higher speeds and a wider operating temperature range and increasingly aggressive synthetic Automatic Transmission Fluids (ATF)
- Produced using proven conventional high volume manufacturing processes
Differentiating factors | HiSpin® PDR RT | HiSpin® HS40 |
---|---|---|
Surface speed |
60 m/s |
40 m/s |
Ability to handle runout |
0.05 max |
0.1 max |
Dry running |
+++++ |
+++ |
Range of fluid compatibility | +++++ |
+++ |
Ease of assembly |
+++ | +++++ |
Temperature range |
-55 °C to +260 °C |
-45°C to +200 °C |
Torque/power consumption |
+++++ |
+++++ |
Ability to handle pressure | +++++ |
+++ |