Taking the Pressure Off Car Batteries

Date: 31.10.18
In the world of automotive innovations, the move toward greater fuel efficiency and thus a smaller environmental impact has led to the widespread use of stop-start technology. Thanks to Trelleborg Sealing Solutions, a small but ingenious valve seal is meeting the considerable demands placed on car batteries by such systems.
IN SHORT
- Pressure build-up is a problem in the car batteries used for stop-start systems
- Ventseal-Light from Trelleborg Sealing Solutions combines a venting and sealing function to overcome this problem
- Demand for the seal is rising along with the number of applications for this type of battery
How Ventseal-Light Works
Ventseal-Light is a patented, low-pressure valve combining excellent impermeability with a secure opening and closing behavior. It is suitable for all cases where the pressure in a closed receptacle must be kept below a certain limit, while at the same time any ingress from the outside has to be sealed off securely. Opening pressures for the valve range from 50 to 400 mbar and it is available in two different types of elastomer material, depending on the pressure requirements and media used. In terms of function and cost, Ventseal-Light is an optimized version of the wellknown Ventseal series.