ROS saves the day by extending the Tractor Warranty!


India, being primarily an agricultural-driven economy, places significant importance on agricultural machinery, particularly tractors. These machines have played a pivotal role in transforming India's agriculture, boosting productivity, and enabling efficient land cultivation. Tractors are no longer a status symbol but have become a necessity for farmers nationwide. However, with increased reliance on this equipment, any downtime can lead to significant losses in terms of both man-hours and crop yields. Therefore, farmers seek low-maintenance and reliable products, considering them as major investments.
To meet these demands, tractor manufacturers strive to make their equipment as robust as possible. Before tractors are deployed in the field, they undergo rigorous testing to ensure their performance in harsh environments. Each component is thoroughly tested before the final product is launched. Manufacturers invest heavily in selecting the right equipment and partnering with Tier 1 and 2 suppliers to ensure product reliability.
Despite these efforts, warranty issues can arise once tractors are released into the market. These issues not only impact the company's reputation but also lead to product recalls and additional maintenance costs. Trust on the Brand is crucial for farmers, and any such issues can significantly impact their purchasing decisions.
One of the leading tractor manufacturers in India faced warranty issues with one of its latest models, particularly concerning the transmission section. According to warranty claims, it was discovered that mud was entering the transmission, particularly the rear lift arm shaft area, causing the tractor to stop. With further investigation customer realized that the O-ring in the shaft was causing the leakage and allowing the mud to enter the transmission system.
Rotary & Shaft Seals
Rotary seals and shaft seals are used in components with oscillating or rotating parts to keep lubrication fluids in while preventing ingress of mud and water. The seal demonstrates superior low-friction properties and provides excellent resistance to wear. They keep oil, and grease in the system, and prevent ingress of dust and dirt. The Rotary Solutions have been proven effective in various market segments, providing superior performance and durability.