Higher reliability and safety for all you food transfers

Date: 10.11.19
Higher Reliability & Safety
Transfer fluids without fear with Trelleborg food hose asemblies. Specially designed to prevent bacterial growth, they have no hidden spaces that can escape cleaning if they are bent or under pressure. Their crimped fittings offer other advantages as well: perfect tightness, which serves to prevent risk of dislocation, even in the most extreme conditions including pressure or temperature. The crimps eliminate protrusions while the ferrule protects the hose end of the assembly. For added protection, the hose assembly has a registration number for traceability.