Key facts

Icon drinking water
2.2 billion people
lack access to safely managed drinking water
Icon sanitation
4.2 billion
people
lack safely managed sanitation
Icon wastewater
80%
wastewater

in the world flows back into the ecosystem without being treated or reused

Icon leaking pipe
Over 35% water
that has been produced is "lost" before it reaches the customer

Our goal: zero leakage

Running water

Pipe & manhole seals and ancillary equipment

A manhole cover

Trenchless pipe repair

Saving every precious drop
Water is the most precious resource we have.

Committed to the sustainable global goals

UN_Goal
UN Goal 6

One of the targets is to improve water quality, wastewater treatment and safe reuse

UN_Goal
UN Goal 9

Build resilient infrastructure, promote inclusive and sustainable industrialization and foster innovation

UN_Goal
UN Goal 11

Make cities and human settlements inclusive, safe, resilient and sustainable