contactusurl/sv-se/seals/searchInga resultatAnimation is not fully supported in Internet Explorer versionsitem founditems founditem foundsidoravSökVisarPå denna sidaÅterförsäljareDistributörOfficial DealerPremium PartneradresseradresserRegulatoriskt pressmeddelande,Regulatory press releases onlyEG. Food Hoses conformity evolution WebinarSelector Button
In this presentation Manuel Funk, Project Development Engineer Healthcare & Medical, Joe Dawber, Manager Custom Product Engineering, and Carolin Grandt, Commercial Director, describe the inquiry and development process of LSR-two-component projects at TSS from the request to the finished series part.
Based on an example, the three experts present the development possibilities of the R&D area (e.g. design layout; FEA etc.), as well as the support from manufacturing site (e.g. flow simulation, tool layout, etc.). Based on this, the presentation will also include the possible manufacturing steps from prototyping to mass production.