Stop the Pressure with Trelleborg Engineered Coated Fabrics and True Source

Using Dartex® by Trelleborg Engineered Coated Fabrics for top covers brings a variety of clinical benefits, as well as comfort for the patient.
What is an alternating pressure mattress?
An alternating pressure mattress is a specialized medical device designed to prevent and treat pressure ulcers.
It achieves this by periodically redistributing pressure across the surface of the mattress.
The internal air cells cyclically inflate and deflate.
This process changes the points of contact between the patient's body and the mattress surface, thereby
Who needs an alternating pressure mattress?
Patients who are at high risk of developing pressure ulcers typically require an alternating pressure mattress.
This includes individuals who are:
- Bedridden or immobile patients who are unable to change their position frequently.
- Elderly, as aging skin is more susceptible to pressure damage.
- Limited or no ability to move parts of their body.
- Suffering from severe illness or injury, resulting in prolonged bed rest.
- Suffering from existing pressure ulcers, as this helps prevent further damage and aid in healing.
Benefits of an alternating pressure mattress
Pressure Relief:
The primary function is to reduce pressure on critical areas of the body, such as the heels, elbows, shoulders, and sacrum.
Dartex® fabrics have stretch and recovery properties, which allows the top cover to move in harmony with the moveable air cells beneath.
Durability and Hygiene:
It is imperative that alternating pressure mattresses are made from durable materials that are easy to clean.
Dartex® fabrics have antimicrobial properties to help prevent infections.
Comfort:
Despite the mechanical operation, the mattress is designed to provide comfort to the patient, often incorporating a soft, breathable cover.
True Source uses Dartex® by Trelleborg Engineered Coated Fabrics, as it is soft and enables envelopment of the body.
Its stretch properties help to distribute the weight of the patient and can enhance higher comfort.
Adjustability:
Customizable settings to cater to the specific needs and preferences of the patient.
Low Air Loss:
Certain models feature low air loss to help manage moisture and temperature, further preventing skin breakdown.
Stop the pressure with True Source
Alternating pressure mattresses play a crucial role in the care of patients at risk for pressure ulcers by providing dynamic pressure redistribution, enhancing comfort, and promoting skin integrity.
These mattresses are essential in both hospital and home care settings for maintaining the health and comfort of vulnerable patients.
https://www.medical-truesource.com/
www.trelleborg.com/en/engineered-coated-fabrics/HM-Range
Lawrence Tan, APAC Business Development Manager, Trelleborg Engineered Coated Fabrics said:
”True Source is a great example of a company that really understands the requirements of the patient.
By choosing to work with Dartex® fabrics from Trelleborg, True Source ensures that the whole mattress system is aligned – the cover and the core working together for the benefit of the patient.”
Cindy Chien, Product Manager, True Source said:
Trelleborg Engineered Coated Fabrics has been a good partner for us for our mattress covers.
Trelleborg understands the requirements of our business and supplies high quality fabrics for our alternating pressure mattresses.
Their technical expertise sets them apart from other fabric providers we have previously used.