Not shook up

When a major seismic event occurs, the tremors and aftershock can be devastating to the communities and infrastructure all around. Fully functional underground pipeline systems are a cornerstone of the modern urban human community, carrying fresh water for drinking and washing, and channeling away both stormwater and sewage. If pipes buckle or burst, the damage can cause critical disruption to society and present a significant danger to public health.
Seismic activity is among the most damaging hazards to buried pipelines. This is particularly the case with shallow seismic events, which are closely associated with the liquefaction of soil; losing its strength and stiffness when shaken, it begins to behave like a liquid. In these situations, pipes can float upward, and joints tend to telescope, buckle and rupture, spilling out their contents and allowing liquefied material to seep into and pollute water.
“Flexible connector seals in infrastructure systems are essential because they allow for lateral joint movement,” says Martijn Boerma, Business Development Manager
for pipe seals in Asia Pacific within Trelleborg Industrial Solutions. Trelleborg offers a series of flexible pipe connectors including the Kor-N-Seal Pipe-to-Manhole
Connector, which is produced in the U.S. and marketed worldwide.
Trelleborg’s F-576 Anger-Lock seals are used in oriented PVC (PVC-O) pipe systems, which are more flexible and the material of choice in New Zealand. “We sell about two million Anger-Locks and almost half a million Kor-N-Seal seals globally every year,” Boerma says. “Our customers know that our high-performance seals will do the job, and in places where earthquakes are common, they consider the investment in our solutions to be worth every penny.”
After the 1995 Kobe earthquake in Japan, an initial inspection of 52 manholes in the municipality – half of them with conventional pipe-to-manhole connections and half with Trelleborg’s Kor-N-Seal flexible connectors – found that the majority of the conventional connections had suffered varying degrees of failure. However, of those featuring Kor-N-Seal connectors, only one was found to have a small leak.
The Japanese government sets high requirements relating to the performance and ease of installation of pipe and joint seals. Today, when old pipes that have sockets with a G-ring become dysfunctional, they are most commonly replaced with pipes fitted with Trelleborg’s integrated seals.
One of Trelleborg’s valued customers in Japan is concrete pipe manufacturer Ito Yogyo.
Chikako Kotani, who works in the development department at Ito Yogyo, says, “Our pipes with Trelleborg’s integrated seals have a longer spigot and socket, providing enough twirls and the required ‘drawing’ amount. These pipes have become popular in the Kinki, Tokai and Kanto districts where many earthquakes occur.”
The islands of New Zealand are situated astride one of the most active tectonic plate boundaries on Earth. From 2010 to 2012, the city of Christchurch was largely destroyed as a result of major earthquakes. Besides natural disasters such as these, shallow tremors occur on a regular basis, and these can have a serious effect on
infrastructure. This is why most counties in New Zealand have switched to relatively flexible PVC-O pipes, fitted with Trelleborg’s unique F-576 Anger-Locks.
Frank O’Callaghan, National Technical Manager at Iplex, one of Trelleborg’s long-term partners in New Zealand, says, “There is simply no such thing as an ‘earthquake-proof’ pipe. However, flexible pipes such as our PVC-O pipes with Anger-Lock seals have generally performed well, with significantly fewer breaks and leaks observed compared with other commonly used nonflexible pipes.”
For more information, please go to:
https://www.trelleborg.com/en/seals-and-profiles
This is an article has been reproduced from Trelleborg's T-Time magazine. To download the latest edition, go to: www.trelleborg.com/t-time
Press Service: This article is available in eight languages. Media are welcome to use this article in their own publications. To download the article and pictures in any language go to https://bamboo-contentpartner.com/. If you reproduce information from this release, please give contact details as: www.trelleborg.com.