Engineering Solutions for Extreme Offshore Environments

FPSO-elastomeric-bearings

This article examines the design of module support bearings for MISC Offshore's new Floating Production, Storage and Offloading (FPSO) project in South America. Trelleborg's marine construction team discusses the technical challenges that were addressed through advanced engineering methods like Finite Element Analysis (FEA) and material science to ensure durability and reliability.

 

In this project, considering the FPSO was situated in waters 2 km deep and prone to tropical storms, strong currents, and saltwater corrosion, what were the main technical challenges in designing bearings for such extreme conditions? How did you address them?
Designing module support bearings for the MISC Mero FPSO in extreme deepwater conditions involves addressing challenges related to corrosion, load management, motion, and maintenance. By selecting suitable materials, design codes, employing advanced design techniques, and integrating innovative solutions, these challenges can be effectively met, ensuring reliable operation in one of the most demanding offshore environments. The result is a robust bearing system capable of withstanding the unique stresses and environmental conditions present in deepwater FPSO operation.

 

Your team employed advanced modeling techniques, including Finite Element Analysis, to predict stress-strain characteristics. How crucial is FEA testing?
FEA simulation and testing are essential in the design and development of offshore structures like the MISC Mero FPSO. It provides critical insights into stress-strain behavior, optimizes designs, enhances safety, and ensures compliance with regulatory standards. By employing FEA, engineering teams can create robust, efficient, and reliable structures capable of withstanding the harsh conditions of deepwater environments, ultimately contributing to the success and safety of offshore operations.

FEA enables the optimization of geometries and materials used in bearings and other components. By simulating different designs, engineers can identify the most efficient and effective solutions. This leads to lighter, stronger components that are cost-effective and meet safety standards without over-engineering, ultimately reducing material costs and weight.

 

The bearings use specially formulated elastomer compounds resistant to oil-based process liquids. Can you discuss the importance of material science in your solutions and how it contributes to the 120-year design life of the bearings? More specifically, for this project, how did using specially formulated elastomer compounds resistant to oil-based process liquids impact longevity/durability?

Material science, particularly the use of specially formulated elastomer compounds resistant to oil-based process liquids, is fundamental to the longevity and durability of bearings in the MISC Mero FPSO project. By ensuring resistance to chemical degradation, enhancing mechanical properties, providing environmental protection, and enabling maintenance-free operation, these materials play a crucial role in achieving the 120-year design life of the bearings. This approach not only enhances operational reliability but also contributes to the overall success of offshore projects in challenging environments. The choice of materials directly influences the performance, longevity, and reliability of bearings in harsh environments. For the Mero FPSO, the bearings were subjected to extreme conditions, including exposure to oil-based process liquids and varying temperatures. Utilizing materials that can withstand chemical exposure, temperature fluctuations, and mechanical stresses is essential for achieving long service. The elastomer compounds specifically designed for this application ensure that the bearings can endure these conditions without significant degradation.

 

How does your team maintain flexibility in complex offshore projects?

Flexibility in complex offshore projects is essential for navigating uncertainties and achieving successful outcomes. By employing agile management practices, fostering collaboration, leveraging advanced technologies, and maintaining proactive risk management, our team is equipped to adapt to changing conditions and stakeholder needs effectively. These strategies not only enhance project resilience but also contribute to the successful delivery of high-quality offshore installations.

 

According to recent market research, the FPSO market is projected to grow from $5.4 billion in 2023 to $13.8 billion by 2032, with a CAGR of 12.50%. How is Trelleborg positioning itself to capitalize on this growth, and what trends do you see driving this expansion?

Trelleborg is well-positioned to capitalize on the growth of the FPSO market through strategic investments in R&D, a commitment to sustainability, and a focus on innovation and technology. By aligning its offerings with the key trends driving market expansion, Trelleborg aims to enhance its competitive advantage and contribute to the success of its clients in the evolving offshore oil and gas landscape. Recognizing the diverse needs of clients, Trelleborg is focusing on providing customized solutions tailored to specific project requirements and environmental conditions. This adaptability helps Trelleborg stand out in a competitive market by offering products that align closely with client needs, thereby enhancing customer satisfaction and loyalty.

 

Looking ahead, what do you envision as the next big technological leap in FPSO design and operation, and how is Trelleborg preparing to meet these future challenges?
The next big technological leaps in FPSO design and operation will be driven by advancements in digital technology, materials science, and sustainability. Trelleborg is actively preparing to meet these future challenges by investing in innovative solutions, collaborating with technology partners, and focusing on safety, reliability, and environmental responsibility. This proactive approach ensures that Trelleborg remains at the forefront of the FPSO market, ready to support its clients as the industry evolves. Trelleborg is proactively preparing for the future of the FPSO market by aligning its products and strategies with key technological advancements. This approach ensures that Trelleborg remains a leader in the industry, ready to support clients as the sector evolves.