Aerospace

As airplane designs focus on flying at higher altitudes and speeds for longer periods, the many hydraulic systems onboard must adapt. Today's conditions can include temperatures above 600°F (315,5°C), temperatures as low as -65°F (-54°C), and pressures up to 5,000 psi (345 bar)
Automotive & eMobility

As the world attempts to reduce its dependence on fossil fuels, biofuels are now a reality. Brazil and the U.S. were early adopters of this alternative fuel for transportation but now its use is expanding in Europe, with Germany, France and Spain leading the way.


By Harlan Hart, technical manager, e-mobility, Trelleborg SealingSolutions.
Recognising that a specialised sealing solution was needed for e-Mobility applications, Trelleborg Sealing Solutions has developed two new seals that could help noticeably extend the distance travelled by electric vehicles between charges, as Harlan Hart, technical manager, e-Mobility, explains

When Electric Vehicles Take Over
By Jeff Kerns, published in "Machine Design Magazine"
Are supply chains, materials, and drivability of EVs helping or hurting?

New Seals Reduce Friction for Electric Vehicle Adoption
By Harlan Hart, Technical Manager, e-Mobility for Trelleborg Sealing Solutions, published in "Machine Design Magazine"
Increasing electric vehicles driving range is more than just a matter of batteries and motors.

As a matter of flat: The importance of high-quality flat seals in chemical transportation
Reprinted with permission from Bulk Transporter. Find the original article at BulkTransporter.com

Secure Transport of Chemicals - Sicherer Transport von Chemikalien
By Marco Schildknecht, Segment Manager Chemical & Processing Europe, Trelleborg Sealing Solutions
Even when exposed to the most aggressive chemicals, the two sealing materials Isolast J9503 and Isolast J9567 perform very well. They seal reliably under extreme conditions and have a long service life.
This article is in German and was originally published in August 2022 in cav - Prozesstechnik für die Chemieindustrie It is reposted by permission, copyrights are reserved to the publication.
Chemical Transportation
Energy

Sealing Considerations for Fire-Safe Valves
A valve that can temporarily survive a fire scenario gives personnel time to escape and find safety. "Fire safe" is the term used to describe valves that survive temperature extremes from a stimulated blaze. They can be choke, ball, gate or other designs and typically operate with a valve stem that rotates, reciprocates or is a quarter-turn type.
By Eric Bucci, Trelleborg Sealing Solutions
Originally published by Chemical Engineering

Bearing considerations for offshore wind platforms
Trelleborg's Orkot composite bearing materials are well suited for demanding high-load applications
like offshore wind platforms.
Byline: Mark Hampton, Product and Innovations Manager, Trelleborg Sealing Solutions
Originally published by Bearing Tips.

Seal testing options for hydrogen storage and transport
As the world transitions towards a net zero future, hydrogen is growing in importance as one of the key elements that will help deliver a more sustainable future.
This article originally published by Design World

Maximizing wind turbine efficiency through optimized hydraulic sealing
Advanced seal designs that prevent wear, increase service life, and reduce friction can ensure uptime in pitch cylinders and brakes.
This article original ran in Sealing & Contamination Control Tips

Minimizing Equipment Downtime with In-situ Seal Welding Technology
The ideal solution is for completion of any seal repairs or replacements on FPSO vessels to be completed offshore, in-situ, to speed up the process and minimize equipment downtime.

Trelleborg introduces XploR S-Seal
By Eric Bucci, published in "Rubber & Plastics News"
Trelleborg Sealing Solutions recently launched XploR S-Seal and XploR FSSeal, extrusion-resistant elastomers the company developed for demanding high temperature and high-pressure sealing environments in the oil and gas industry.

Trelleborg's tensioner cylinder seals exceed 20-year lifecycle rating
By Mary Gannon
Seals used in offshore rig tensioner cylinders must meet the same rigorous lifecycles as the
cylinders themselves. Because offshore environments are harsh and installation and maintenance
can be difficult, tensioner cylinders must have a 20-year life. That was why, more than 20 years
ago, Trelleborg Sealing Solutions conducted research, determining that its seals could last this
necessary lifecycle.

Perfluoroelastomer (FFKM) elastomers offer exceptional thermal stability, outstanding long-term compression set and almost universal chemical compatibility – delivering long life in the most aggressive of media, including hydrocarbon and aqueous media, common within oilfield applications.

As the oil and gas industry evolves, sealing materials are required to work effectively in more challenging environments. This article details the effects of exposure to water-based hydraulic fluids and High-Pressure/High-Temperature (HPHT) fields on common sealing materials.
Fluid Power & Off-Highway

Aiding in the Balancing Act: Removing the Burden of Innovation for Fluid Power Customers
By Michael Cook, Global Segment Director Off-Highway, Trelleborg Sealing Solutions. Originally published by Fluid Power Journal
We need to look at ways to help each other formulate new solutions with minimal effects on daily business operations. One way to do this is by pursuing a shared innovation approach across the fluid power supply chain.

Simulations reveal valuable information about Fluid Power Components
This article was originally published in the Fall/Winter 2023 issue of Your World in Motion and is shared with permission from the Canadian Fluid Power Association (CFPA). To learn more about CFPA and to read the full issue at no cost, visit https://cfpa.ca/.
To achieve optimal efficiency, fluid power applications and their sealing components need good friction characteristics and long life to reduce maintenance. Engineering simulations can help original equipment manufacturers (OEMs) succeed in an environment where the demands for efficiency are increasing.

Why stocking standard products pays off for OEM and supplier relationships
By Scott Christensen, originally published by "Sealing & Contamination Control Tips"
Original Equipment Manufacturers (OEMs) and their tier suppliers rely on sealing partners for a wide range of services and capabilities. An experienced and knowledgeable sealing supplier can provide everything from high-quality custom sealing solutions and FEA analysis to online tools and resources for engineers.

All Around the World: Circular Sustainability for Fluid Power
In today’s environmental and economic landscape, it is critical for fluid power component manufacturers and seal suppliers to incorporate sustainable methods into design, manufacturing, and production practices through design thinking for circularity and circular products.
This article was originally published in the November 2022 issue of Fluid Power Journal

Spotlight on Sealing Solutions for Fluid Power and Off-Highway
Ensuring performance in extreme conditions, industrial seals meet unique application needs.

No-Leak Zone: The Mighty Mechanical Face Seal
Mechanical Face Seals, also called lifetime seals, floater seals, duo cone seals or toric seals are important to the long-life function of heavy equipment in agriculture, construction and mining.

Advancements in Double-Acting Rotary Seals Prove More Effective
By Beth Figliulo, Fluid power segment manager, published in "Electronic Component News", Dec. 2018
How specialized Rotary Seals are alleviating fluid power pressure build-up for high-speed, high-pressure applications

Modern machinery, equipment and motors fitted with hydraulic cylinders are becoming more powerful, which means that the hydraulic systems therein are increasingly subject to higher operating pressures and temperatures.

The right seal reduces contamination in hydraulic systems
Learn what causes contamination and how to choose seals that protect against it.

Zero-Leak Wipe Systems Fluid 'Weepage'
Hybrid robots combining hydraulic and electric systems are becoming more common in assembly lines and warehouses. Hybrid hydraulic and electrical designs require special care when specifying hydraulic sealing systems because weepage of even a light coating of hydraulic fluid can negatively affect electrical system performance.
This article was originally published in the February 2022 issue of Fluid Power Journal. It is reposted by permission.

High Modulus Plastics Can Play a Key Role in Off-Highway Vehicles
By Tom Zozokos, Product Line Director, and Beth Figliulo, Fluid Power Segment Manager Americas, Trelleborg SealingSolutions.
Co-injection molding is one technology of interest for those designing hydraulic systems for off-highway use. This allows two polymers to be combined in a single operation to create multiple functions in one component.

Boosting performance in hydraulic systems with alternative coatings
By Beth Figliulo and Michael Cook, Trelleborg SealingSolutions.
Taking a holistic approach to sealing solutions in hydraulic systems using chrome alternatives helps engineers achieve optimum function.

Materials for Maximum Wear Ring Performance
Published in "Flow Control", May 2018
Read how Wear Rings can extend the life of a hydraulic system
Food & Beverage Processing

Processing Q&A: Rotary fillers with Trelleborg's Caio Beraldo
Each piece of equipment and machinery used in the food and beverage processing industry is different and has a unique set of sealing requirements. Caio Beraldo, technical manager for food, beverage and water at Trelleborg, discusses the uses and sealing needs for rotary fillers.
This article appeared on Processing Magazine’s website

Processing Q&A: Horizontal mixer sealing with Trelleborg's Caio Beraldo
From mixers and food pumps to valves and fillers, the range of equipment and machinery used in the food, beverage and water industry is diverse. Each has its own set of sealing requirements and understanding these critical components takes expertise.
This article appeared on Processing Magazine’s website

Processing Q&A: Vertical mixer sealing with Trelleborg's Caio Beraldo
Trelleborg's Technical Manager for Food, Beverage and Water, recently connected with Processing to discuss the uses and critical sealing components for vertical mixers.

Selecting the right seals for food and beverage processing
Understanding common seal materials and factors that affect performance can help ensure the seling solution best meets the requirements for the application

Engineered Solutions for Smart Appliances with LSR Processing
The Research and Markets Institute (researchandmarkets.com) projects the global household appliances industry to reach an estimated value of US$ 324.2 billion by 2019. Amongst the major drivers are growing affluence of the middle-class population in emerging markets, higher disposable incomes, and more per capita spent on lifestyle products in increasingly urbanized environments.

Product change without aroma carryover (Language: German)
Trelleborg Sealing Solutions has partnered with Krones, a specialist in beverage bottling, to analyze the reasons behind unintentional flavor carryover during the filling process. The companies found elastomer sealing components to be a relevant factor in aroma carryover and that the selection of the optimum sealing material is crucial in preventing the transfer of flavors from one filling process to the next.

David Kaley — Trelleborg Sealing Solutions; Edited by Mike Santora
With stainless steel and other metals so predominant in industrial food manufacturing equipment, it may seem unusual to suggest a more significant role for plastic wear rings and bearings. But for a broad range of food production and transportation machines, advanced polymers are an effective way to reduce friction and handle load instead of traditional metal bearings.

Trelleborg Seals help keep food and beverage industry clean
By David Kaley, published in "Rubber & Plastics News"
One of the most important aspects for the food and beverage industry is sterility. Preventing cross-contamination on the plant floor is crucial. Any company creating pieces of equipment needs to adhere to the industry's strict regulations.

Smart Engineering Solutions for Smart Appliances with LSR Processing
By Ursula Nollenberger, published in "appliance DESIGN"
The global household appliances industry is seeing a steady influx of technologically advanced appliances that deliver innovative, smart features to save the user time and make life more comfortable. This article demonstrates the role custom-engineered LSR parts have in this segment.
Industrial Automation

Trelleborg shares Insights on Sealing Needs for Electric Motors
Originally published by Power Transmission Engineering
From electric motors and linear actuators to robots and gearboxes, the range of equipment and machinery used to crate automation in industrial applications is divers. Each has its own set of sealing requirements and understanding these critical components requires many years of experience. In this article David Kaley, Trelleborg's global segement manager for industrial automation, shares his insights on sealing needs for electric motors.

Motors and More: Achieving Greater Effieciency in Industrial Automation Applications
Originally published on Automation.com
Industrial automation is highly beneficial because it decreases production times, improves quality and increases productivity in a world where
customers expect quick turnaround times.

By Darren Conway, Global Product Line Director, Trelleborg Sealing Solutions
Many industrial sectors, including aerospace, semiconductor, automotive and biopharmaceutical, require rotary seals as original equipment manufacturers (OEMs) switch from hydraulic to electric motor systems for greener solutions and improved product performance.
Polymer Materials

High-Performance Plastics: The Value and Challenges of High-Volume Precision Molding
The use of high-performance thermoplastics can reduce time and expense during design, prototyping and manufacturing. They are recyclable, able to bond to differing materials and lighter than their steel counterparts.
Originally published by Machine Design

There is no one-to-one replacement
What opportunities and risks the seal supplier Trelleborg sees in the impending ban on PFAS substances (per- and polyfluoroalkyl substances), which is causing nervousness among manufacturers, processors and users.

This is the way—to safe chemical transport
By Thijs Menzel. Reprinted with permission from Bulk Transporter Magazine. Find the original article at BulkTransporter.com
Chemical compatibility, material testing, root cause failure analysis among the critical keys to success, sealing expert says

The right seals and materials keep chemicals moving
ByThijs Menzel
The world relies on chemicals to provide the essentials of modern life and they are the basic building blocks of everyday items; from the fertilizers that help grow our food to the beds we lie on, from the shoes on our feet to the cars that we drive. Transporting those chemicals safely to where they are needed, is a major logistical effort that requires advanced sealing technology.

Published on "ChemInfo", May 2018
The chemical compatibility of a seal with the fluids in a system is critical to obtaining a reliable, long-lasting seal. Here are some considerations for choosing the right material for a given chemical sealing application.

Polyurethane (PU) materials offer outstanding wear, extrusion and abrasion resistance with good elasticity and low compression set.

Looking Beyond Chemical Compatibility Charts: Matching Plastic and Elastomer Seals with Fluids
By Lucy Heyduk and Tim McCulfor, Trelleborg Sealing Solutions
Chemical compatibility charts are often used as a quick and concise way to match the proper fluid with a seal. However, there is much more to consider with the chemical compatibility of a seal in relation to the fluids in a system. This information is critical to gaining a reliable and long-lasting seal — and the selection process can be daunting.
Seal Design & Technology

Where the rubber meets the road for component design and manufacturing
The development of a custom rubber seal can be challenging.
Relying on industry specialists and considering potential manufacturing
methods and production volumes will enable you to navigate the
innovation process.
This article was first published in Design World.

Inventory Management Systems Play an Essential Role Now and Into the Future
As the economy reopens and demand for manufactured products returns to normal, it has become challenging to manage inventory of the parts needed for production. While no one product or service can solve all of these problems, inventory management systems have become an increasingly useful tool for managing labor and supply chain issues. This article reviews the current situation and how one new automated inventory management system can help alleviate some of the pain of C-Class inventory management.

Composite Simulation Grows MORE ROBUST
By Kenneth Wong
The transition from metal to composite is one of the most recent significant changes in manufacturing.
The former material is isotropic, exhibiting uniform stretching and bending behavior in all directions. By contrast,composites are anisotropic. They stretch, bend and break differently in different directions, based on how the fibers are woven together and how the laminates are bonded. This fundamental difference throws many traditional simulation protocols and practices into chaos.

Reduce Vibration and Avoid Stiction in Seals
By Holger Jordan, fluid power segment manager, Trelleborg Sealing Solutions
Stick-slip is not always a big issue, but sometimes it can significantly
degrade performance. Potentially, it can cause damage, such as cracks in
steel work and strength loss, and even health problems for operators.
We look at solutions to combat stick-slip to lower vibration as well as to create damping solutions.

When one is better than many
By Ursula Nollenberger; Trelleborg Sealing Solutions; Published in “MEDengineering” (edition 2/2020)
As medical devices become ever more sophisticated and smaller in size, the challenge for the component manufacturer is how to fit multiple functions into a limited space. Multi-component LSR technology offers a solution to this, that in addition, provides designers with the latitude and flexibility to enhance their applications.

By Michael Cook and Kelly Volpenhein; Published in "Fluidpower Journal"
This article was originally published in the February 2019 issue of Fluid Power Journal. It is reposted by permission.

With global engineering and production facilities, state of-the-art cleanrooms and advanced automated processes, Trelleborg Sealing Solutions already offers its medical device, biotech and pharmaceutical customers specialized custom molded solutions that enhance their product offerings.
Semiconductor

Damping within Vacuum for Front-end Semiconductor Processes
By Kevin Kaufenburg, Semiconductor Business Development Specialist, Trelleborg Sealing Solutions
Manufacturing the latest design of tiny transistors presents challenges for semiconductor original equipment manufacturers (OEMs). As transistors shrink beyond ten nanometers, vacuum environments for semiconductor processes play a critical role...
This article was originally published by Semiconductor Digest.
Healthcare & Medical

Providing Biopharmaceutical Manufacturers with Cutting-Edge Material and Assembly Solutions
Article originally published in BioProcess International
Trelleborg experts leverage a reinforced polypropylene (PP) composite material´to make thin, light chromatography columns, using significantly less material than is needed for traditional options.

Device Development Excels in Rapid Development Centers
Design and material choices can have a long-term impact on manufacturing costs and effieciencies for medical device manufacturers. When they work together with experienced component manufacturers from the start of a project, they can save time, reduce costs, and produce premium quality products, while keeping an eye on the goal of a smooth transition to serial production.

Handy medical devices make life easier for people with chronic conditions, and automated dosing systems are gradually replacing regular injections of essential medication. Trelleborg cooperated with WACKER to develop a microinjection pump, the very heart of such devices.

Single-Use Systems: The Future of Biopharmaceutical Processing
Single-Use systems represent the future in biopharmaceutical processing of therapeutic drugs with significant advantages
over traditional reusable stainless-steel systems and partly disposable systems.

Q&A: Reducing the cost of long-term manufacturing
Medical Plastic News spoke with Chris Tellers, Rapid Development Center director, Trelleborg Healthcare & Medical to learn out about the company's recently launched Rapid Development Center in Delano, Minnesota
Water & Sanitary

Addressing Sealing Challenges Associated with Smart Meters
Smart gas meters enable companies, households and municipalities to remotely access data and device functionality through a network, such as Wi-Fi, a portal or a cellular phone network. The U.S. smart meter market is projected to reach $7.69 billion by 2027 at a CAGR of 10.47%, according to Allied Marketing Research.
By Jerry Schmitz, Global Segment Director, Trelleborg Sealing Solutions